FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > Gestures available for the document display function
FAQ
Gestures available for the document display function
What gestures are available for the document display function?
Answer
The following gestures are available for the document display function.
• Swipe: Scroll or change the page in the direction swiped (eight directions)
• Pinch in: Zoom out (25% to 400%)
• Pinch out: Zoom in (25% to 400%)
*1: For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (document display)
- Series
- GOT3000 Series