Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 45478
  • Release Date : 2025/11/12 13:54
  • Print

Regarding maximum number of years of clock data that can be handled

What is the maximum number of years that the clock function of the FX5 CPU module can handle? Also, what happens if the number of years is exceeded?

Category : 

Answer

The  maximum number of years of the clock function is 2079 years.
If it exceeds the maximum number of years, it will be fixed at 23:59:59 on December 31, 2079.

Product Name
FX5U,FX5UC,FX5UJ,FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries