FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding checking the input/output data of the FX5-EIP
FAQ
Regarding checking the input/output data of the FX5-EIP
How can I check the connection status and input/output data from GX Works3 to FX5-EIP?
Answer
This can be checked by monitoring the corresponding buffer memory from the Register to Intelligent Function Module Monitor.
From [Parameter] - [Module Information] in the navigation window of GX Works3, right-click FX5-EIP and select "Register to Intelligent Function Module Monitor."
- Product Name
- FX5-EIP
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series