• No : 20775
  • Release Date : 2018/08/21 16:10
  • Update : 2018/09/07 12:40
  • Print

About coasting time

Answer

The coasting time is the time from when the brake power is turned off until the brake starts braking. The coil has the characteristic that electric current tries to flow even after abrupt power supply cut.
Therefore, in case of simultaneous breaking method, circulating current is generated in the motor coil and the brake coil, and the coasting time becomes longer.
Product Name
Geared Motors
Series
Geared Motors Parallel shaft type, Geared Motors Right angle shaft type, S-PM Geared Motors Parallel shaft type, S-PM Geared Motors Right angle shaft type