• No : 20776
  • Release Date : 2018/08/21 16:10
  • Print

Brake operation when electrical power is on or off

Answer

The braking method of the geared motor with a built-in brake is a frictional disk type direct current electromagnetic brake, non-excitation braking method (spring braking method).
Therefore, it is a safety brake that applies brakes when power failure occurs.
Product Name
Geared Motors
Series
Geared Motors Parallel shaft type, Geared Motors Right angle shaft type, S-PM Geared Motors Parallel shaft type, S-PM Geared Motors Right angle shaft type