- No : 20776
- Release Date : 2018/08/21 16:10
-
Print
Brake operation when electrical power is on or off
Does the brake operate regardless of whether electrical power is on or off?
- Category :
-
Answer
The braking method of the geared motor with a built-in brake is a frictional disk type direct current electromagnetic brake, non-excitation braking method (spring braking method).
Therefore, it is a safety brake that applies brakes when power failure occurs.
- Product Name
- Geared Motors
- Series
- Geared Motors Parallel shaft type, Geared Motors Right angle shaft type, S-PM Geared Motors Parallel shaft type, S-PM Geared Motors Right angle shaft type