- No : 21123
- Release Date : 2018/08/22 16:26
-
Print
Multi-speed setting
When Pr.24 (4 speed) of multi-speed setting is only set and RH, RM, RL are all turned ON, which frequency is applied for the operation?
- Category :
-
Answer
If Pr 27 is not set, the operation starts at the speed of RL.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ