- No : 21144
- Release Date : 2018/08/22 16:26
-
Print
Wiring length
What is the total wiring length when an inverter and a terminal block are connected with a wire of 100m and a terminal block and five motors are connected with wires of 20m for example?
- Category :
-
Answer
The total wiring length is as follows: 100 m + (20 m × 5) = 200m.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ