- No : 21261
- Release Date : 2018/08/22 16:26
-
Print
Operation panel (DU04)
Is the parameter unit FR-DU04 available in the 700 series inverters?
- Category :
-
Answer
The FR-DU04 can be used in the 700 series inverters, however, some restrictions apply and parameter copy is disabled.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700