• No : 21263
  • Release Date : 2018/08/22 16:26
  • Print

Amount of heat generated

Answer

Refer to the FR-A700/F700/E700/D700 series TECHNICAL MANUAL (section 3.7.2) and the Technical News. The FR-A700/F700/E700/D700 series TECHNICAL MANUAL can be downloaded from the Mitsubishi Electric FA Global Website. - FR-A700/F700/E700/D700 series TECHNICAL MANUAL Select FA HOME > Inverters-FREQROL > Technical manual (It is displayed by clicking "Select large category".) FR-A700/F700/E700/D700 series TECHNICAL MANUAL: SH-060014 - Technical News FA HOME > Inverters-FREQROL > Technical library > Technical news MF-Z-078: FREQROL-A700 series amount of heat generated (Amount of heat generated for other models are also described.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700