- No : 21267
- Release Date : 2018/08/22 16:26
-
Print
Frequency setting signal
While the current 4 to 20 mA is input to terminal 4, the FWD blinks and operation does not start. Pr.267 (Terminal 4 input selection) is set to "0" and voltage/current input selection switch of terminal 4 is turned ON ("I" for E700 and D700). What are the possible causes for this?
- Category :
-
Answer
Check the AU signal (AU - SD). To use the terminal 4, the AU signal (AU - SD) needs to be turned ON. Turning ON the AU signal (AU - SD) disables the terminal 2.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700