- No : 21268
 
      - Release Date : 2018/08/22 16:26
 
        - 
          
              Print
          
        
 
  
 
Frequency setting signal
    
      I want to set 0 Hz for 4 mA and 50 Hz for 20 mA while the current 4 to 20 mA is input to terminal 4. Which parameters should I set?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Set C5 (Pr.904) (Terminal 4 frequency setting bias frequency) to 0 Hz and Pr.126 (Terminal 4 frequency setting gain frequency) to 50 Hz.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700