• No : 21268
  • Release Date : 2018/08/22 16:26
  • Print

Frequency setting signal

I want to set 0 Hz for 4 mA and 50 Hz for 20 mA while the current 4 to 20 mA is input to terminal 4. Which parameters should I set?
Category : 

Answer

Set C5 (Pr.904) (Terminal 4 frequency setting bias frequency) to 0 Hz and Pr.126 (Terminal 4 frequency setting gain frequency) to 50 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700