- No : 21271
- Release Date : 2018/08/22 16:26
-
Print
Motor coasting
How can I set the motor to coasting state?
- Category :
-
Answer
To set the motor to coasting state, the following methods are available: 1. Set Pr.250 (Stop selection) to "0" and turn OFF the start command.
2. Short the terminals MRS and SD.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700