• No : 21281
  • Release Date : 2018/08/22 16:26
  • Print

Speed command

When analog input is used for the speed command, the motor is driven because a little voltage is output with the potentiometer set to 0.
Category : 

Answer

Calibrate the terminal 2 bias.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700