• No : 21283
  • Release Date : 2018/08/22 16:26
  • Print

Life diagnosis

In the life check function for the main circuit capacitor, how is the life diagnosis performed?
Category : 

Answer

When Pr.259 (Main circuit capacitor life measuring) is set to "1", the life diagnosis is ready.
Turning OFF the power supply starts measuring the life of the capacitor.
The life is determined according to the decreasing rate and time.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700