• No : 21288
  • Release Date : 2018/08/22 16:26
  • Print

Switching between External operation mode and PU operation mode

Answer

Assign X16 signal, and set Pr.79 to "0", to switch the operation mode with turning ON/OFF X16 signal.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700