- No : 21288
- Release Date : 2018/08/22 16:26
-
Print
Switching between External operation mode and PU operation mode
I want to switch the External operation mode and PU operation mode with the switch.
- Category :
-
Answer
Assign X16 signal, and set Pr.79 to "0", to switch the operation mode with turning ON/OFF X16 signal.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700