• No : 21291
  • Release Date : 2018/08/22 16:26
  • Print

Electronic thermal O/L relay

When the motor with 0.2 kW is used, trips occur frequently due to the electronic thermal O/L relay error.
Can I set the operation time of the electronic thermal O/L relay?
Category : 

Answer

Check that the correct rated motor current is set in Pr.9 (Electronic thermal O/L relay).
No parameter is available for setting the operation time of the electronic thermal O/L relay.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700