• No : 21302
  • Release Date : 2018/08/22 16:26
  • Print

FR-PA07

When using the option FR-PA07 and external terminals, how do I switch the setting dial and multi-speed selection?
Category : 

Answer

Since the multi-speed is given a higher priority, the setting by the setting dial is not enabled unless all of the multi-speed signals are OFF.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700