• No : 21304
  • Release Date : 2018/08/22 16:26
  • Print

FR-PA07

Is the FR-E5P (back cover and adapter) provided with the FR-E500 necessary for the option FR-PA07?
Category : 

Answer

Since the FR-PA07 has the back cover and adapter, the FR-E5P is not necessary.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700