- No : 21313
- Release Date : 2018/08/22 16:26
-
Print
Supported model for FR-Configurator
The models other than FR-A700/F700 cannot be selected in FR-Configurator (FR-SW2-SETUP-WJ).
How can I select it?
- Category :
-
Answer
For the models other than FR-A700/F700, use FR-Configurator (FR-SW3-SETUP-WJ).
They are not supported by FR-Configurator (FR-SW2-SETUP-WJ).
When you have the FR-SW2, it can be updated by downloading FR-SW3 from the Mitsubishi Electric FA Global Website.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700