- No : 21314
- Release Date : 2018/08/22 16:26
- 
          
              Print
          
        
 
Supported model for FR-Configurator
    
      Is the FR-E700 supported by FR-Configurator (FR-SW2-SETUP-WJ)?  
    
  
    - Category : 
- 
      
    
 
    Answer
  
    The FR-E700 is not supported by FR-SW2-SETUP-WJ. 
The FR-E700 series are supported by FR-SW3-SETUP-WJ. 
This software can be downloaded from the Mitsubishi Electric FA Global Website. 
If you have FR-SW2-SETUP-WJ, it can be updated.
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700