- No : 21314
- Release Date : 2018/08/22 16:26
-
Print
Supported model for FR-Configurator
Is the FR-E700 supported by FR-Configurator (FR-SW2-SETUP-WJ)?
- Category :
-
Answer
The FR-E700 is not supported by FR-SW2-SETUP-WJ.
The FR-E700 series are supported by FR-SW3-SETUP-WJ.
This software can be downloaded from the Mitsubishi Electric FA Global Website.
If you have FR-SW2-SETUP-WJ, it can be updated.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700