• No : 21315
  • Release Date : 2018/08/22 16:27
  • Print

Printing files saved in the previous version of FR-Configurator

Can I print the parameter file of FR-SW3 using FR-SW2 in FR-Configurator (FR-SW3-SETUP-WJ) Ver.2.00?
Category : 

Answer

The parameter file of FR-SW3 cannot be printed using FR-SW2.
The latest version of FR-SW3 can be downloaded from the Mitsubishi Electric FA Global Website. Update FR-SW2 to FR-SW3.
Match the version of FR-Configurator when using it.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700