• No : 21334
  • Release Date : 2018/08/22 16:27
  • Print

Pulse change

When the output frequency is output from the terminal FM, the value stops when the maximum frequency is reached.
The pulse is counted and displayed.
When the frequency is 60 Hz, 1440 pulses are output. Can I change the number of pulses at 60 Hz?
Category : 

Answer

When the pulse is counted and displayed, 1440 pulses are output with the frequency of the inverter is 60 Hz. Since these pulses are limited to 2400 pulses, and the value stops when the maximum frequency is reached.
The number of pulses at 60 Hz can be changed with Pr.55 (Frequency monitoring reference) as the frequency for 1440 pulses.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700