• No : 21335
  • Release Date : 2018/08/22 16:27
  • Print

Parameter display setting

When Pr.80 (Motor capacity) and Pr.81 (Number of motor poles) are set, "Er4" is displayed and the settings are disabled.
How can I set them?
Category : 

Answer

Normally, Pr.80 and Pr.81 are the parameters that can be changed when the operation is stopped in the PU operation mode.
The "Er4" is a mode designation error. Check the operation mode.
When Pr.79 is set to "2", the parameter setting cannot be changed since External operation mode is activated.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700