• No : 21341
  • Release Date : 2018/08/22 16:27
  • Print

Instruction manual

I have purchased the inverter but only the Instruction Manual "Basic" was included.

How can I get the Instruction Manual "Applied"?
Category : 

Answer

For the Instruction Manual "Applied", fill in the request sheet which is included in the last part of the Instruction Manual "Basic", and fax it to the specified phone number. Then we will send the "Applied" version to you.
We can also send it via your sales agent.
(The instruction manual can be downloaded from the Mitsubishi Website. Registration is required.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700