• No : 21342
  • Release Date : 2018/08/22 16:27
  • Print

Wiring the terminal

I use the 24 VDC power supply of the terminal PC with a 24 VDC relay across the terminals PC and RUN and terminals across SD and SE shortened.
Is there any problem with the wiring?
Category : 

Answer

There is no problem with the wiring.

Keep the rating (24 VDC, 0.1 A) of the terminal PC.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700