• No : 21344
  • Release Date : 2018/08/22 16:27
  • Print

Applied terminal

When connecting a potentiometer with the terminals 10, 2, and 5 of the inverter, do I have to use the shielded cable?
Category : 

Answer

As described in the instruction manual, use the shielded cable or twisted cable to avoid the influence of noises.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700