- No : 21348
- Release Date : 2018/08/22 16:27
-
Print
Frequency setting
It is described that the initial setting of up to frequency operation range is "10%". Is the up to frequency signal output at 6 Hz when the running frequency is 60 Hz?
- Category :
-
Answer
For the set frequency 60 Hz, ±6 Hz is applied and thus the up to frequency signal is output between 54 Hz and 66 Hz.
During acceleration/deceleration to the allowable range, the signal is turned OFF.
The signal is turned ON during operation within the allowable range.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700