- No : 21362
- Release Date : 2018/08/22 16:27
-
Print
FR-PA07
When using the enclosure surface operation panel FR-PA07, is the adapter necessary?
- Category :
-
Answer
The adapter is not necessary. Only the dedicated cable FR-CB20□ is required.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700