• No : 21364
  • Release Date : 2018/08/22 16:27
  • Print

FR-PA07

Can I perform the forward rotation and reverse rotation by pressing the FWD/REV key on the enclosure surface operation panel FR-PA07?
Category : 

Answer

The forward rotation and reverse rotation are enabled by pressing the FWD/REV key on the operation panel.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700