• No : 21675
  • Release Date : 2018/08/22 16:28
  • Print

Network operation

Can I switch between external operation and network operation by setting Pr.182 (Terminal RH function selection) to "66" (External-NET operation switching)?
Category : 

Answer

Yes.

With the setting "66", you can choose NET operation when X66 is ON, and external operation when X66 is OFF.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700