• No : 21686
  • Release Date : 2018/08/22 16:28
  • Print

Switching between external operation and NET operation

To switch external operation and NET operation, I set Pr.181 (Terminal RM function selection) to "66", Pr.79 (Operation mode) to "0", and Pr.340 (Communication startup mode selection) to "1". Can I monitor the fault output in both NET operation and external operation?
Category : 

Answer

You can monitor the fault output in both NET operation and external operation.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700