- No : 21695
 
      - Release Date : 2018/08/22 16:28
 
        - 
          
              Print
          
        
 
  
 
PU operation
    
      Pressing the PU/EXT button does not switch to PU. I want to change the frequency. 
An external start command is used and the frequency is set with the setting dial.
PU, EXT, and MON turn ON.
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    If Pr.79 = 3, PU and EXT turn ON. Switching between PU and EXT is not available. Turn the setting dial to set the frequency and press the SET key to accept it.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700