• No : 21717
  • Release Date : 2018/08/22 16:29
  • Print

Motor specifications setting

Although I will use the inverter with the power supply voltage three-phase 240 VAC/60 Hz, I want to get 200 V/60 Hz output.
Is it possible to configure the inverter for this?
Category : 

Answer

Yes.

Set Pr.19 (Base frequency voltage) to "200 V".

200 V output will be obtained during 60 Hz operation.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700