• No : 21724
  • Release Date : 2018/08/22 16:29
  • Print

Electromagnetic contactor

Is it possible to avoid open/close surges of the electromagnetic contactor by setting the inverter parameters?  
Category : 

Answer

It cannot be avoided by using parameters.  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700