• No : 21727
  • Release Date : 2018/08/22 16:29
  • Print

10 VDC voltage from terminal 10

I cannot get 10 VDC voltage from the terminal 10 even after changing Pr.73 (analog input selection) to "0" (for 0 to 10 V input). Is this a failure?  
Category : 

Answer

Setting Pr.73 to "0" does not generate 10 VDC output.

The inverter itself only has 5 V at the terminal 10.

Setting this parameter to "0" allows 10 V input between the terminals 2 and 5 from an external power supply. The FR-A700/F700 (P) can output 10 VDC voltage from the terminal 10E.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700