• No : 21731
  • Release Date : 2018/08/22 16:29
  • Print

Automatic restart after instantaneous power failure setting

Is setting Pr.162 (automatic restart after instantaneous power failure selection) enough to set the automatic restart after instantaneous power failure function?  
Category : 

Answer

You also need to set Pr.57 (Restart coasting time).

The function does not work just by setting Pr.162 unless setting this parameter.
(For A700, F700, and F700P, terminals CS and SD must be short-circuited.

Use the input terminal function assignment parameter to set the terminal CS.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700