• No : 21738
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

Answer

You can set the running frequency up to 400 Hz.

It depends on the specifications of the motor used whether or not operation with a frequency of 120 Hz or higher is available.
Such operation is available with a high-speed motor.

Use Pr.18 (Maximum frequency) to set the maximum frequency.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700