- No : 21739
- Release Date : 2018/08/22 16:29
-
Print
Frequency setting
When setting the frequency, I set a frequency with the setting dial, press the SET key, and then press the RUN key to operate the inverter. Can I change the frequency during operation?
Currently, I stop the inverter before changing the frequency.
- Category :
-
Answer
Even while the inverter is operating, you can use the setting dial to change the frequency and then press the SET key and the inverter operates at the new frequency.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700