• No : 21745
  • Release Date : 2018/08/22 16:29
  • Print

Frequency, monitor setting

Using external signals for operation allows for monitoring the running frequency, and I want to continuously monitor the setting frequency.
How should I configure the setting?
Category : 

Answer

Set Pr.52 (PU/DU main display data selection) to "5".

Set the monitor as the third monitor, frequency -> current -> setting frequency.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700