- No : 21764
 
      - Release Date : 2018/08/22 16:29
 
        - 
          
              Print
          
        
 
  
 
Monitor indicator
    
      How can I switch the monitor display from the output frequency to output current?  
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Press the "SET" key once while the output frequency is monitored.
The unit indicator LED changes from "Hz" to "A" and the monitor display changes to the current.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700