- No : 21764
- Release Date : 2018/08/22 16:29
-
Print
Monitor indicator
How can I switch the monitor display from the output frequency to output current?
- Category :
-
Answer
Press the "SET" key once while the output frequency is monitored.
The unit indicator LED changes from "Hz" to "A" and the monitor display changes to the current.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700