• No : 21765
  • Release Date : 2018/08/22 16:29
  • Print

Monitor indicator

I want to check the frequency on the monitor but when I set the running frequency and operate the inverter, the monitor shows the current (A).   
Category : 

Answer

The first priority window of the monitor may be set to the current.

When the current is displayed on the monitor (the unit is "A"), press "SET" to switch to the voltage monitor window (no unit), and then press "SET" again. The frequency is shown on the monitor (the unit is "Hz").

If you want to set the frequency as the first priority, press and hold the "SET" key for a while.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700