• No : 21771
  • Release Date : 2018/08/22 16:29
  • Print

Terminal setting

I want to use the terminal 4 of the inverter as the voltage input terminal. How should I configure the setting?
Category : 

Answer

To use the terminal as voltage input, you need to:
- Set Pr.267 (Terminal 4 input selection).
- Set the voltage/current input switch on the inverter board.
- Set the short-circuit of the terminals AU and SD.

Pr.267 selects the input voltage from 0 to 5 V and 0 to 10 V.
Set the switch to the "V" (voltage) side.
Assign the terminal AU (Terminal 4 input selection) to an unused terminal.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700