• No : 21773
  • Release Date : 2018/08/22 16:29
  • Print

Multi-speed setting and external potentiometer

Answer

The multi-speed setting is prioritized.

The external potentiometer setting is effective when the multi-speed signal is not input.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700