- No : 21775
- Release Date : 2018/08/22 16:29
-
Print
Operation panel
I input the start signal via the terminal STF and set the frequency using the setting dial. I set Pr.161 (Frequency setting/key lock operation selection) to "1" (potentiometer mode) and Pr.79 (Operation mode) to "3".
When I press the "STOP" key on the operation panel, the motor is decelerated to stop and "PS" and "0.00" blink on the monitor. What happened?
- Category :
-
Answer
This is because the protective function works to stop the motor. It is not a fault indication.
To cancel the protective function, turn OFF the start signal and press the "PU/EXT" button.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700