• No : 21779
  • Release Date : 2018/08/22 16:29
  • Print

Output current value

Can I change the detection level of the output current value using a potentiometer or something similar?
Category : 

Answer

The detection level of the output current value cannot be changed using a potentiometer or a similar device.  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700